AD9361 External Reference clock XTALN Pin signal range

Hi,

We are planning to operate AD9361 with external 10MHz Sinewave OCXO clock using single ended  XTALN (Pin M12) and XTALP (Pin M11) is not connected (leave floating).

In the datasheet it was mentioned the input clock Signal Level 1.3 Vp-p (AC-coupled external oscillator) which in 50Ohms load +6.3dBm.

But in the datasheet there is no minimum and maximum and absolute maximum rating levels for this clock source pin. Please provide the values for the same.

Regards,

Sugumar K