AD9361 Bypass Capacitors on +1.3V Rail

Hello,

I was wondering what the recommended bypassing is for the VDD_RX_SYNTH and VDD_TX_SYNTH rails as well as the other +1.3V rails.  On the FMCOMMS3 board it seems like for those only a 1uF and 0.01uF cap are needed as close to each ball (J3/K3) as possible.  In other reference designs, it shows a 10uF and 0.01uF.  What is the recommended bypassing scheme?  Is there an application note that describes in detail what size capacitors/capacitance is needed for each of the balls?