AD9361 in LVDS mode

Hi,

I need some clarification about the max data sampling rate in a 2R configuration for the LVDS mode.

The max data clock rate in LVDS mode is 245.76 MHz.. I understand that in this mode, the

IQ samples are transmitted on the dedicated P1 port in the following sequence :

I1msb, Q1msb, I1lsb, Q1lsb, I2msb, Q2msb, I2lsb, Q2lsb (figure 79 of UG 570).

I conclude that the max IQ sampling rate in LVDS mode is 245.76/8 = 30.72 MHz. and not 61.44 MHz.

Is that correct ?

What will be the maximum RF bandwith in this case ?

Thanks