l_clk, clk and div_clk settings when using 4 chips. 2 of 4 chips in 1r1t mode

In my design I have 4 axi_ad9361 IPs to connect to 4 chips.  2 of these chips will only have 1 receive channel.  So, on these two chips I was going to set the 1r1t parameter to '1'.

axi_ad9361_0 - 2 receivers

axi_ad9361_1 - 1 receiver

axi_ad9361_2 - 2 receivers

axi_ad9361_3 - 1 receiver

Option 1: Can I connect l_clk from axi_ad9361_0 to the clk inputs on all 4 chips? Would I need to set the 1r1t parameter to 0 on all 4?

Option 2: Do I connect l_clk from axi_ad9361_0 to axi_ad9361_0 clk and axi_ad9361_2 clk and l_clk from axi_ad9361_1 to axi_ad9361_1 clk and axi_ad9361_3 clk?  Will I need two util_clk_dividers and two separate fifos (one fifo for ad9361_0,2 and one fifo for ad9361_1,3)?

Top Replies