ad9361 tx power of BW 20MHz

Hi ad9361 experts:
   I read the datasheet, and I want to confirm one thing. When the tx bandwidth is 20MHz, the tx attenuation is 0dB, and the tx lo frequency is 1.44GHz, what will the output power of ad9361 be? According to my test, it` s about -20dBm. Is this normal?

Thanks a lot.

Parents
  • 0
    •  Analog Employees 
    on Jan 14, 2019 9:37 AM

    The output power depends on the type and the level of the signal that you are giving at input.

    As per the datasheet, the max tx output power is 7.5dBm at 2.4GHz with a 1MHz tone at input.

    We do not confirm on any data apart from the datasheet.

Reply
  • 0
    •  Analog Employees 
    on Jan 14, 2019 9:37 AM

    The output power depends on the type and the level of the signal that you are giving at input.

    As per the datasheet, the max tx output power is 7.5dBm at 2.4GHz with a 1MHz tone at input.

    We do not confirm on any data apart from the datasheet.

Children