ADALM-PLUTO: 3.8 GHz or 6 GHz?

The data sheets say the top end is 3.8 GHz but in the videos on YouTube Robin Getz says 6 GHz and therefore it works for 5 GHz WiFi.

Which is correct?

Also many of the ADALM-PLUTO tutorial and document links are 404. Some say they are under development or redesign. Will there be any self-taught course or tutorials for this product? It seems like a great idea... but only with good documentation and tutorials. I'm interested in using as a WiFi sniffer, spectrum analyzer, and diagnostic tool in areas of high ambient RF at 2.4 and 5 GHz as well as LoRa at 915 MHz. Thanks...

Parents Reply Children