Internal PLL IN AD9361

Hello

i would like to know about the lock time of the ad9361?

and the time he can switch freq ?

Parents
    •  Analog Employees 
    on Aug 22, 2019 6:40 AM

    PLL cal + lock times depend on the configuration of the chip.

    Below are examples of cal +lock times:

              fref          TDD          FDD

         19.2MHz     ~105us     ~525us

         40MHz        ~60us      ~260us

         80MHz        ~55us      ~140us

    If you want faster frequency switching time, then you can use the fast lock feature available in which the previously stored profiles are recalled and hence the frequency change time is reduced to only the synth lock time (typically 15us-20us).

Reply
    •  Analog Employees 
    on Aug 22, 2019 6:40 AM

    PLL cal + lock times depend on the configuration of the chip.

    Below are examples of cal +lock times:

              fref          TDD          FDD

         19.2MHz     ~105us     ~525us

         40MHz        ~60us      ~260us

         80MHz        ~55us      ~140us

    If you want faster frequency switching time, then you can use the fast lock feature available in which the previously stored profiles are recalled and hence the frequency change time is reduced to only the synth lock time (typically 15us-20us).

Children
No Data