Post Go back to editing

Question on how to receive ORX data through JESD after DPD operation in ADRV9029

Category: Software
Product Number: ADRV9029
Software Version: SW6.2.0.35

It is set to 3pin ORx Selection mode as shown in the figure below.

However, although I enabled it on the RXx_en pin, ORx Data is not coming in through JESD.

I know that no ORX data is coming out through JESD during DPD operation.

But I want to receive ORX data through JESD when DPD operation is finished, please advise on how to control it.

Thank you for your support.



add
[edited by: Justin.Jung at 2:23 AM (GMT -4) on 27 Jun 2022]

Top Replies

Parents
  • However, although I enabled it on the RXx_en pin, ORx Data is not coming in through JESD.

    You are using a link sharing profile so the ORX data comes on JESD only when the TX is on.

    I know that no ORX data is coming out through JESD during DPD operation.

    Yes, but the other ORX side of the chip can get the JESD data.

    See below:

    When ORX_CTRL_A is high and based on CTRL_B and CTRL_C logics, the respective ORX data goes to the JESD and on the other ORX side of the chip, the DPD cal will run.

  • TXx_en is correct, not RXx_en. I wrote it wrong by mistake.

    Currently, in 3pin mode, DPD from Tx1 to 4 is operating normally.

    Can I know when the link sharing ORx data comes out through JESD after the ORx path is used by the DPD actuator? (Time to capture ORX in FPGA is limited, so please inquire.)

    Additionally, when DPD is executed on ORx1,2, ORX data should appear on ORx3,4, but ORX data is not displayed through JESD.

    In this regard, please let me know if there is anything I need to check or if there is any data needed to analyze this issue.

  • While the DPD is running on one side of the ORX, the other side of the ORX data will be available on the JESD.

    Is the other side of the ORX data is available through your external path routing for the FPGA on the JESD?

    Is your Use case has ORX enabled?

Reply Children