Post Go back to editing

Question about RXx_en pin function of ADRV9026

Category: Datasheet/Specs
Product Number: ADRV9026

Hello,

My customer use ADRV9026 in their system.

And now they are testing with ADI EVM for checking functions and performances of ADRV9026.

Below is a question form them.

During then, RXx_en is able to control Rx channel ON/OFF.

If RXx_en is Rx channel off, ADC in RX channel is off or not.

 

They  want know the state of ADC when RXx_en is disabled.

Would let me know your answer?

Regards,

Se-woong

Top Replies

    •  Analog Employees 
    Jun 9, 2022 in reply to Se-woong +1 verified
    It meanse that when RXx_en pin is  off, it is the output of Rx channel with ADC alive or with ADC off.

    No, there wont be any data alive on the ADC when the Rx channel is off