Hi,test environment: the signal is 5gnr 100M bandwidth, the frequency point is 3.65g, 4tx / Rx / 4orx, and the DPD function of adrv9025 works normally in FDD working mode. However,in TDD mode, the DPD working state of the same link is different after each power on. Sometimes the DPD function is normal after power on, and sometimes the DPD function does not work and the signal does not converge after power on. The DPD state when it does not converge is shown in the figure below
The DPD parameters:
dpdIndirectRegularizationValue=20
dpdDirectRegularizationValue=35
dpdSamples=16384
#dpdMThreshold=((10^MThreshold_dBFS/20)*FULL_SCALE_CODE)^2
MThreshold_dBFS=-21
FULL_SCALE_CODE=32768
dpdPeakSearchWindowSize=655350
dpdUpdateMode=1
minAvgSignalLevel=2560
#Default value
dpdMu=50
minAvgSignalLevelOrx=512
dpdFilterSel=0
enableDirectLearning=0
dpdIndirectRegularizationLowPowerValue=20
question:How can we avoid the error 0x340a of dpd and make the DPD function normally In TDD working mode
Thank you.