DEARS.
When booting with Tx= PLL2, Rx= PLL1 settings, only PLL2 is detected as Locked and PLL1 is detected as Unlocked.
Any problem with the file below?
Thank you
DEARS.
When booting with Tx= PLL2, Rx= PLL1 settings, only PLL2 is detected as Locked and PLL1 is detected as Unlocked.
Any problem with the file below?
Thank you
The limitation could be coming from the integer / fractional synthesizer mode of the PLL. What is the reference clock in your setup? Refer page 75 of the UG for more details.
Can you change the PLL1 frequency to 3761 or 3760 and see if the LO is getting locked?
Hi
Could I set each channel for different frequency look like Tx1 to 900Mhz
Tx2 to 1800Mhz
Tx3 to 12500Mhz
and Tx to 3.5 Ghz
Many thanks
Rich
No, that's not possible as the chip does have only 2 LOs.
Hi
Any possibility to use external LO?
Best Regards
Rich
No, the chip does not support External LO
Many Thanks
Many Thanks