Post Go back to editing

Questions related to DPD model sweep script execution

Hello?

wiki.analog.com/.../dpd_model_optimization

As in the link above, I ran the DPD model sweep script, but only the following results are displayed and no further progress is made.

Connected
***************************************
Setting up DPD Tracking Config
DPD Tx Low Power Threshold(dBFS) =  -36.0056515422
DPD M Threshold(dBFS) =  -2.00000000595
DPD Peak Search Window Size =  491520
DPD Regularization Value =  25
DPD Samples =  16384
DPD Update Mode =  ADI_ADRV9010_DPD_TRACKING_UPDATE_MODE_0
***************************************
Num Models =  140
Num coeffs read from file =  95
Asserting Full DPD Reset
Enabling DPD Tracking Cal
Microsoft.Scripting.ArgumentTypeException: expected adi_adrv9025_DpdStatusX_t, got adi_adrv9010_DpdStatus_t
   at Microsoft.Scripting.Interpreter.ThrowInstruction.Run(InterpretedFrame frame)
   at Microsoft.Scripting.Interpreter.Interpreter.Run(InterpretedFrame frame)
   at Microsoft.Scripting.Interpreter.LightLambda.Run5[T0,T1,T2,T3,T4,TRet](T0 arg0, T1 arg1, T2 arg2, T3 arg3, T4 arg4)
   at System.Dynamic.UpdateDelegates.UpdateAndExecute4[T0,T1,T2,T3,TRet](CallSite site, T0 arg0, T1 arg1, T2 arg2, T3 arg3)
   at Microsoft.Scripting.Interpreter.DynamicInstruction`5.Run(InterpretedFrame frame)
   at Microsoft.Scripting.Interpreter.Interpreter.Run(InterpretedFrame frame)
   at Microsoft.Scripting.Interpreter.LightLambda.Run2[T0,T1,TRet](T0 arg0, T1 arg1)
   at System.Dynamic.UpdateDelegates.UpdateAndExecute3[T0,T1,T2,TRet](CallSite site, T0 arg0, T1 arg1, T2 arg2)
   at Microsoft.Scripting.Interpreter.DynamicInstruction`4.Run(InterpretedFrame frame)
   at Microsoft.Scripting.Interpreter.Interpreter.Run(InterpretedFrame frame)
   at Microsoft.Scripting.Interpreter.LightLambda.Run2[T0,T1,TRet](T0 arg0, T1 arg1)
   at IronPython.Compiler.PythonScriptCode.RunWorker(CodeContext ctx)
   at Adi.Tpg.IronPythonWindow.ScriptHost.Execute(String expression)

Please advise.