DEARS.
We have confirmed the normal operation and performance of DPD with the settings below.
General System Specifications
Freq: 889Mhz
BW: 10MHz
DPD Info: UC50_Nonlinksharing, Gen3 model 67
However, when I input the signal source as ETM2, it works abnormally.
DPD Status is 0x341d.
To check if it is an AMP problem, I tested with the configuration below.
ADRV9025 TX -> ADRV9025 ORX
DPD Status is the same as 0x341d.
How do I get it to work with ETM2?
Thank you.