I am trying to use WOLFSPEED(CREE)'s GTRB424908FC for AMP
However, STABILITY_ERROR is continuously displayed on DPD Status.
Can I get some advice on this?
Please help.
thank you.
I am trying to use WOLFSPEED(CREE)'s GTRB424908FC for AMP
However, STABILITY_ERROR is continuously displayed on DPD Status.
Can I get some advice on this?
Please help.
thank you.
You are getting stability error because of high EVM and select errors. Update count is 0 means DPD tracking never updated.
try attached model file.
0 0 0 0 0.0 0.0 0 0 1 0 0.0 0.0 0 0 2 0 0.0 0.0 0 0 3 0 0.0 0.0 0 0 4 0 0.0 0.0 0 0 5 0 0.0 0.0 0 0 6 0 0.0 0.0 1 0 2 1 0.0 0.0 1 0 3 1 0.0 0.0 1 0 4 1 0.0 0.0 1 0 5 1 0.0 0.0 1 0 6 1 0.0 0.0 1 0 8 1 0.0 0.0 2 0 1 2 0.0 0.0 2 0 2 2 0.0 0.0 2 0 3 2 0.0 0.0 2 0 4 2 0.0 0.0 2 0 5 2 0.0 0.0 2 0 7 2 0.0 0.0 2 0 8 2 0.0 0.0 3 0 1 3 0.0 0.0 3 0 2 3 0.0 0.0 3 0 3 3 0.0 0.0 3 0 4 3 0.0 0.0 3 0 6 3 0.0 0.0 3 0 7 3 0.0 0.0 3 0 8 3 0.0 0.0 4 0 2 4 0.0 0.0 4 0 3 4 0.0 0.0 4 0 4 4 0.0 0.0 4 0 5 4 0.0 0.0 4 0 6 4 0.0 0.0 4 0 7 4 0.0 0.0 4 0 8 4 0.0 0.0 5 0 1 5 0.0 0.0 5 0 2 5 0.0 0.0 5 0 3 5 0.0 0.0 5 0 4 5 0.0 0.0 5 0 5 5 0.0 0.0 5 0 6 5 0.0 0.0 5 0 7 5 0.0 0.0 5 0 8 5 0.0 0.0 6 0 1 6 0.0 0.0 6 0 3 6 0.0 0.0 6 0 4 6 0.0 0.0 6 0 7 6 0.0 0.0 6 0 8 6 0.0 0.0 1 1 0 8 0.0 0.0 1 1 1 8 0.0 0.0 1 1 2 8 0.0 0.0 1 1 3 8 0.0 0.0 1 1 4 8 0.0 0.0 1 1 5 8 0.0 0.0 1 1 6 8 0.0 0.0 1 1 7 8 0.0 0.0 1 1 8 8 0.0 0.0 1 1 9 8 0.0 0.0 1 1 10 8 0.0 0.0 1 1 11 8 0.0 0.0 1 1 12 8 0.0 0.0 2 1 1 9 0.0 0.0 2 1 2 9 0.0 0.0 2 1 3 9 0.0 0.0 2 1 4 9 0.0 0.0 2 1 6 9 0.0 0.0 2 1 7 9 0.0 0.0 2 1 8 9 0.0 0.0 3 1 1 10 0.0 0.0 3 1 2 10 0.0 0.0 3 1 3 10 0.0 0.0 3 1 5 10 0.0 0.0 3 1 6 10 0.0 0.0 3 1 7 10 0.0 0.0 3 1 8 10 0.0 0.0 4 1 1 11 0.0 0.0 4 1 2 11 0.0 0.0 4 1 3 11 0.0 0.0 4 1 4 11 0.0 0.0 4 1 5 11 0.0 0.0 4 1 6 11 0.0 0.0 4 1 7 11 0.0 0.0 5 1 1 12 0.0 0.0 5 1 2 12 0.0 0.0 5 1 3 12 0.0 0.0 5 1 4 12 0.0 0.0 5 1 5 12 0.0 0.0 5 1 6 12 0.0 0.0 5 1 7 12 0.0 0.0 5 1 8 12 0.0 0.0 6 1 2 13 0.0 0.0 6 1 3 13 0.0 0.0 6 1 5 13 0.0 0.0 6 1 6 13 0.0 0.0 6 1 7 13 0.0 0.0 6 1 8 13 0.0 0.0 0 2 2 14 0.0 0.0 0 2 4 14 0.0 0.0 0 2 5 14 0.0 0.0 0 2 6 14 0.0 0.0 0 2 8 14 0.0 0.0 2 2 0 15 0.0 0.0 2 2 1 15 0.0 0.0 2 2 2 15 0.0 0.0 2 2 3 15 0.0 0.0 2 2 4 15 0.0 0.0 2 2 5 15 0.0 0.0 2 2 6 15 0.0 0.0 3 2 1 16 0.0 0.0 3 2 3 16 0.0 0.0 3 2 4 16 0.0 0.0 3 2 5 16 0.0 0.0 3 2 6 16 0.0 0.0 3 2 7 16 0.0 0.0 3 2 8 16 0.0 0.0 4 2 2 17 0.0 0.0 4 2 3 17 0.0 0.0 4 2 4 17 0.0 0.0 4 2 6 17 0.0 0.0 4 2 7 17 0.0 0.0 6 2 1 26 0.0 0.0 6 2 2 26 0.0 0.0 6 2 3 26 0.0 0.0 6 2 5 26 0.0 0.0 6 2 6 26 0.0 0.0 6 2 7 26 0.0 0.0 6 2 8 26 0.0 0.0 0 3 2 18 0.0 0.0 0 3 3 18 0.0 0.0 0 3 6 18 0.0 0.0 0 3 7 18 0.0 0.0 0 3 8 18 0.0 0.0 1 3 1 19 0.0 0.0 1 3 2 19 0.0 0.0 1 3 4 19 0.0 0.0 1 3 6 19 0.0 0.0 1 3 7 19 0.0 0.0 1 3 8 19 0.0 0.0 2 3 1 20 0.0 0.0 2 3 2 20 0.0 0.0 2 3 3 20 0.0 0.0 2 3 5 20 0.0 0.0 2 3 6 20 0.0 0.0 2 3 7 20 0.0 0.0 2 3 8 20 0.0 0.0 3 3 0 21 0.0 0.0 3 3 1 21 0.0 0.0 3 3 2 21 0.0 0.0 3 3 3 21 0.0 0.0 3 3 4 21 0.0 0.0 3 3 5 21 0.0 0.0 3 3 6 21 0.0 0.0 6 3 1 27 0.0 0.0 6 3 2 27 0.0 0.0 6 3 3 27 0.0 0.0 6 3 4 27 0.0 0.0 6 3 6 27 0.0 0.0 6 3 8 27 0.0 0.0 4 4 0 22 0.0 0.0 4 4 1 22 0.0 0.0 4 4 2 22 0.0 0.0 4 4 3 22 0.0 0.0 4 4 4 22 0.0 0.0 4 4 5 22 0.0 0.0 4 4 6 22 0.0 0.0 6 4 1 28 0.0 0.0 6 4 2 28 0.0 0.0 6 4 3 28 0.0 0.0 6 4 5 28 0.0 0.0 6 4 6 28 0.0 0.0 6 4 7 28 0.0 0.0 5 5 0 23 0.0 0.0 5 5 1 23 0.0 0.0 5 5 2 23 0.0 0.0 5 5 3 23 0.0 0.0 5 5 4 23 0.0 0.0 5 5 5 23 0.0 0.0 5 5 6 23 0.0 0.0 0 6 1 24 0.0 0.0 0 6 2 24 0.0 0.0 0 6 5 24 0.0 0.0 0 6 6 24 0.0 0.0 0 6 7 24 0.0 0.0 0 6 8 24 0.0 0.0 6 6 0 29 0.0 0.0 6 6 1 29 0.0 0.0 6 6 2 29 0.0 0.0 6 6 3 29 0.0 0.0 6 6 4 29 0.0 0.0 6 6 5 29 0.0 0.0 6 6 6 29 0.0 0.0
Few other things to try out.
If you operate the PA at lower power are you able to get better updates.
Please check the picture below to make sure you did as you advised.
I have also loaded the file you gave the DPD GMP model.
However, STABLITY_ERROR is still occurring on TES.
Please advise on what I can do more.
Currently I am running a DPD model sweep script to find the best model.
Please advise on what I can do more.
Please try with DPD update Mode 2 which is recommended for GaN PA ( GTRB424908FC)
Can you check DPD performance at 'Target power- 3dB'and check if you are still getting stability error?
Lowering the output power (increasing the TX attenuation from 1dB to 10dB) still gives the DPD stability error.
Please advise on what I can do more.
Try Mode 2 as well.
Can you add 10dB attenuator at the ORX input Port of the EVB and check?
Also, can you decrease the ORX Gain Index and try?
I proceeded to DPD Mode 2, but I keep getting STABLITY_ERROR as shown below.
I also attached a 10dB fixed attention to the ORX Port.
Direct EVM comes out about 10%, but if you adjust TX Attenuation and ORX gain, only +/-1% changes.
Thanks for your advice.
I hope you are following the DPD sequence in the GUI, attached for your reference.
Can you run the DPD once by disconnecting the PA, which means Tx to ORX through a coupler (Make sure the ORX is not saturating) and check if you are still seeing stability error ?