Post Go back to editing

ADRV9025 init-Madura

DEARS.

I know that if there is an RF signal input to RX when initializing ADRV9025, fail occurs in the initializing stage of Init-madura.

We inquire about the threshold value that occurs when the signal input to the ADRV9025 RX is at what level.

Thank you.

Parents
  • During the calibrations, the input port should be isolated from the incoming signals and the calibration tones will appear on the Rx pins and, therefore, must be prevented from reaching the antenna through the Rx port being properly terminated.

    The calibrations will be impacted even if there are some low level signals present as well and hence it is recommended that there should not be any signals present on the Rx. pins.

Reply
  • During the calibrations, the input port should be isolated from the incoming signals and the calibration tones will appear on the Rx pins and, therefore, must be prevented from reaching the antenna through the Rx port being properly terminated.

    The calibrations will be impacted even if there are some low level signals present as well and hence it is recommended that there should not be any signals present on the Rx. pins.

Children