about stream image generation

Hello,

I have a question about the stream image generation of adrv9025.

I selected UseCase 51C-NLS in TES and changed the JESD parameters,
but the exported stream image file was the same before and after the change.
This change is to add a lane to the framer[1] and connect Orx to it.

When I read the chapter "Stream Processor and System Control" in the UG-1727,
I found the following are examples of how the stream files can differ:
 The framer choices for ORx and Rx

Why doesn't the stream image change when I change the Orx parameter in framer?
Also, when changing Orx pass from disable to enable, is there a problem if the stream image is not changed?

Thanks,



I've revised the text I posted.
[edited by: takashi1 at 7:50 AM (GMT -4) on 30 Sep 2021]