Hi ADI:
I want to setting ORX to pin mode . I choose Single Channel 1 Pin Mode, and want to enable all orx channel
In the Table 112 in UG1727, it statements a single channel is selected through the API ,
Could you tell me what is the API? And is it possible to enable 4 orx ports simultaneously?
Thanks a lot~
-----------------------------------------------------------------------------------------------------------------------------------------------
UG1727 Table 112:
Single Channel
1-Pin Mode In this mode a single channel is selected through the API (over SPI). ORX_CTRL_A is the enable/disable control pin,
when high the selected ORx is enabled, when low, all ORx paths are disabled. Figure 57 illustrates Single Channel 1 Pin
Mode. Note that ORx1 has been shown in this example, however any of ORx1 to ORx4 can be chosen.