Post Go back to editing

ADRV9026

ADRV9026 evaluation board need FPGA motherboard ADS9-V2EBZ which must be connected to the PC through ethernet. API calls are generated by the PC which is used to program the ADRV9026.
We have few queries:
1.    Instead of displaying the receiver signal on the PC, we want to transmit that signal to other FPGA connected with the ADS9-V2EBZ. How that can be done?
2.    Can other FPGA instead of ADS9-V2EBZ be connected directly with the ADRV9026 evaluation board and can it is possible to program using APIs.

Parents Reply Children