How can you generate a TX signal using IQ data of an RX signal?

The procedure tested is as follows

1. Using SG, the modulation signal was generated in the receiver GUI window

2. Store the generated signals in the form of IQ data

3. Afterwards, the transmit GUI attempts to load data previously stored in IQ format to generate a sigal

4. But, when executed, the following error window occurs "unable to tranmit data, Please check log for details"

I want to know what caused it.

I attach the log file and Stored IQ data form. Please check it.

 - the error log : GUI log.txt

- IQ data of RX signal : RX1_RX1.txt

GUI Log.txt
2020-03-20 15:38:50,610 [ERROR] ERROR	 PerformTx() failed. Exception message: Index was outside the bounds of the array.
System.IndexOutOfRangeException: Index was outside the bounds of the array.
   at System.Array.InternalGetReference(Void* elemRef, Int32 rank, Int32* pIndices)
   at System.Array.GetValue(Int32 index)
   at adrv9010_dll.SubClasses.Fpga9010TxExt.TransportSet(adi_fpga9010_JesdInfo_t jesdInfo, Byte[] dataBytes, List`1& data)
   at adrv9010_dll.SubClasses.Fpga9010TxExt.TxDataSet(adi_fpga9010_JesdInfo_t jesdInfo, adi_fpga9010_TxDatamoverSel_e txDatamoverSel, List`1 data)
   at adrv9010_dll.TopLevelClasses.AdrvDaughterCard.PerformTx(adi_fpga9010_TxTollgateTrigSources_e trigSource, List`1 txData, UInt32 channelMask, Byte continuous)
   at adrv9010_dll.TopLevelClasses.AdrvDaughterCard.PerformTx(adi_fpga9010_TxTollgateTrigSources_e trigSource, List`1 txData, UInt32 channelMask)
   at Adi.adrv9010.ApiCalls.Api.PerformTx(List`1 dataArray, String triggerName)

 
 Please Clear Logs and API errors and try again. 

RX1_Rx1.txt



tag
[edited by: lallison at 6:52 PM (GMT 0) on 25 Mar 2020]