ADRV9008-1 RF_EXT LO export divider

Hello.

 

It is my understanding that the RF_EXT_LO_I/O pins can be used to export a divided version of the VCO for debug purposes. 

 

Does the ADRV9008-1 have seperate dividers for the the RF_EXT_LO export and the internal LO used by the receive path?

 

For instance, lets say that the LO frequency is 2GHz.  The ADRV9008-1 synthesiser will be operating at 8GHz and a divide by 4 will be in place to generate 2GHz.  Is it possible for me to set the divider on the RF_EXT_LO export to be 2, such that I can export 4GHz?

 

Graphically, is this configuration possible?

 

SYNTH(8GHz)  ------|DIV 4|---------> 2GHz LO used by the ADRV9008-1 receive path internally
      |
      |------------|DIV 2|---------> 4GHz exported out of RF_EXT_LO pins

Thanks for the help!

Parents Reply Children