Hi
I want to know how can I enable external LO for adrv9009 eval board with ZC706 and no-os driver? I have set the rfPllUseExternalLo =1; but this causes
error: TALISE_waitInitCals() failed
Thanks
Hi
I want to know how can I enable external LO for adrv9009 eval board with ZC706 and no-os driver? I have set the rfPllUseExternalLo =1; but this causes
error: TALISE_waitInitCals() failed
Thanks
Hi imBilal ,
I can't answer the question directly but I might have an idea which could be of help:
- using TES GUI, generate one profile with internal LO
- using TES GUI, generate another profile with external LO (I guess the GUI offers this possibility)
Do a diff between the two profiles and see if anything else changed, or just rfPllUseExternalLo changed.
In any case I'm moving this thread to design support forum.
Thanks buha
Earlier I posted this question in design forum, but there was no significant answer and it was moved to no-os driver forum. In no-os forum, the question is sitting since one week and there is no reply on that.
So I decided to ask a new question in no-os forum. But now again it is being moved to the same old forum.
I will try your method and let you know in a while.
--
Bilal
Below is the thread for the previous question. I have discussed the problem in detail here:
ADRV External LO as Input; procedure
Pl take a look.
Thanks
Can you disable the Init cals while enabling EXTLO during initialization and check whether EXT LO is working or not . Try this at 1GHz LO frequency .
Also ensure that you are giving 10MHz External reference from REFCLK source to EXT LO source.