Post Go back to editing

ADRV9009 and ADRV9008-1 pinout compatibility

Category: Hardware

Hello,

is it possible to use an ADRV9009 on a pcb designed for the ADRV9008-1?

From the data sheets, it seems this is supported, e.g. the 9009 TX Out pins are DNC and ORX in pins are grounded, on the other hand the SERDIN pins would all be hard pulled up to 1.3V -

will this work hardware-wise, or would I destroy the ADRV9009?

many thanks and greetings

Andreas

Parents Reply Children
No Data