ADRV9009 ADC / JESD: RX Data Path Endianness

Hello,

what is the endianness  of the ADRV9009 ADC data that comes into the JESD?

I'm using the default configuration of JESD (fig.34 in UG-1295).

I want to try to add my own ip in the RX data path in the correct manner.

What i know for certain is that the format is 16 bit signed using 2's complement, but in order to assemble the numbers correctly I'd need the endianness as well.

Cheers!

Parents Reply
  • Hi!

    Thanks for the answer. I assume since the default configuration is 16 bits sample, actually the data is not split into octets and comes into the CPACK2 and out:

    LSByte --------------------------------------- MSByte
    
    Icr0[0-15]   Qcr1[16-31]   Icr3[32-47]    Qcr4[48-63]

    I've observed the data with ILA and the above seems to be correct.

    Would it be possible to confirm my understanding?

Children