Hello Team.
We are reviewing the ADRV9008-1 and ADRV9008-2.
We have some questions.
1. RF_EXT_LO_IO
- Should this port always be used? If this is not used, should the internal RF LO SYNTHESIZER be used?
2 Independent frequency using.
- Can input and output frequency be used independently for each port?
Ex)
==> ADRV9008-1 : RX1_2.4GHz, RX2_5GHz
==> ADRV9008-2 : TX1_2.4GHz, TX2_5GHz
Thank you.
Best & Regards,
Josh.