The Talise Design Package provides s1p files for ORX, Rx, and Tx ports. But do you have them also for the External LO port? Or maybe it is the same as the Rx port? Any data or guidance would be appreciated.
Thanks,
- Jon
The Talise Design Package provides s1p files for ORX, Rx, and Tx ports. But do you have them also for the External LO port? Or maybe it is the same as the Rx port? Any data or guidance would be appreciated.
Thanks,
- Jon
We are checking on this. Will get back to you at the earliest.
Or if you have the data used to generate Figure 451 in the ADRV9009 datasheet, that would work well:
We are checking on this. Will get back to you at the earliest.
I apologize for the delay here.
Please refer to the attached .s1p file for your reference and the updated .s1p plot below.ADRV9009_Ext_LO_Port_Z_at_Ball_Pad_Interface_R0.zip