Is there any model for ADRV9009 in matlab ? If not, at least a behavioural model for the ADC inside ADRV9009 ?

I am trying to use ADRV9009 for receiving a signal of bandwidth 2GHz. My thought was to use 200MHz bandwidth everytime and stitch all the frequency responses later. For this to happen, I need to be clear that the ADC can reject the aliases properly. May I know if there's any model for the ADC or adrv9009 itself ?