Hello,
I am working with ADRV9009 and the Xilinx ZCU102 board for RF PLL hopping. I went through the RF PLL hopping section in UG1295 document. I see that the hopping time given is around 70 micro seconds in specifications. I am using Firmware 6.0.2 and API 3.6.0.1055531162664960005 version. I am testing with NON-GPIO mode and I am observing the transmitter output in Spectrum analyzer in zero span mode. I am clearly abe to measure the hop time taken. It is taking around 100msec.
Is the 100millisecond hopping time acceptable in NON-GPIO mode? What are the expected hopping time in both NON-GPIO mode and GPIO mode?
Yes,NON-GPIO mode or API mode will take additional time due to the SPI writes. You can test using GPIO mode.
API mode is working fine for me. But for GPIO mode I followed the steps given in UG1295 but I am not seeing any frequency hop happening. There are no error values thrown even in SDK code during runtime. I have routed the MIO pins in ZYNQ to GPIO pins of the ADRV9009. This connection is through the FMC connector. After calling TALISE_setFhmHop() function I am making respective MIO pin that is connected to mention GPIO pin on the ADRV board low and then high.
Am I missing anything?
Refer to below link:
https://ez.analog.com/wide-band-rf-transceivers/design-support-adrv9008-1-adrv9008-2-adrv9009/f/q-a/122267/fhm-gpio-mode/374990#374990