Does ADRV9008 DC offset calibration suitable in 5G with subcarrier at DC

Hi expert,

As I known from ug1295 the ADRV9008 hardware reference manul, DC calibration include RF and digital DC offset calibration. But I don't know exactely the procedure of the calibration, like if the radio is off during init calibration and tracking calibration. The reason why I want to know that is I want to know if the DC offset calibration is suitable in 5G with subcarrier at DC. Should I disable this DC offset calibration function or disable during tracking calibration.

Thanks