Minimum Rx sampling rate supported by ADRV9009

Hi,

While the filter wizard tool configuration user guide mentions the minimum Rx RF BW supported by ADRV9009 as 5MHz with the minimum sampling rate as 25MHz, the filter wizard tool is throwing error "Rx output rate should be greater than 39.063MHz and less than 370MHz. The Rx output rate was 30.72". What is the actual minimum rate supported by ADRV9009? Could the ADRV9009 able to support 5MHz Rx RF BW?