Hi everyone,
I am trying to use Fast Frequency Hopping with GPIO trigger mode.
I have this schema:
*** High on the GPIO pin => LO switch to fhm_init_frequency chn_trx_lo.attrs['frequency_hopping_mode'].value = freq_A *** High on the GPIO pin => LO switch to fhm_init_frequency chn_trx_lo.attrs['frequency_hopping_mode'].value = freq_B *** High on the GPIO pin => LO switch to freq_A chn_trx_lo.attrs['frequency_hopping_mode'].value = freq_C *** High on the GPIO pin => LO switch to freq_B
I want to hop to frequency "freq_A" right after setting it or later to "freq_B" but not to the previous registered frequency. Indeed, in this mode, the LO hops twice to the init frequency set in adi,fhm-mode-fhm-init-frequency_hz..
I have seen that in API mode it is possible to hop to the latest supplied frequency instead of the previous registered. But in this mode the hopping is too slow.
Thanks in advance,
D
What are your FHM settings in device tree? I assume what you want is the FHM cal to happen at boot?
-Travis
Frist of all, thanks for your response.
Sencond,
I have not modified any FW, I am using the latest SD Image release 2019_R1 RC.
1.- What FHM calibration does? I have not found any information on that.
2.- I want this schema, in FHM GPIO mode:
Thanks,
Thanks. How fast were you able to set the LO PLL ?
It looks like this was running over an IP connection. I was able to get my frequency hop code working over an IP connection in Python, but it only went from taking 0.3 seconds to taking 0.1 seconds with FHMmode. I would like to be able to set the LO PLLin ~1ms. The UG-1295 hardware guide says you can get down to about 60us, so I would think 1ms should be achievable, but my 100ms number is way off from this.
I'm working on porting the python code from Windows with an IP connection,to the target Linux environment. THis should provide some speed improvement but I'm not sure how much. Any idea here?
After that if that is not fast enough, I will port to C then see how fast that is.
Do you know if the LO PLL loop bandwidth has to be adjusted in FHM mode or is it automatic?
Nathan
NathanB said:I'm working on porting the python code from Windows with an IP connection,to the target Linux environment. THis should provide some speed improvement but I'm not sure how much. Any idea here?
Yes, the software layer could add more delays.
Are you using GPIO or GPIO mode?
NathanB said:Do you know if the LO PLL loop bandwidth has to be adjusted in FHM mode or is it automatic?
Loop Filter is taken care by FHM mode.
Hi,
I'm trying to speed up the FHM, LO changes. I've ran Python code in host and target of the ADRV9009-ZU11EG, but both changes together take about 200 ms (100ms per part) to change the LO frequency in FHM mode. Do you know if a C code implementation would speed this up? (I'm not sure how much over head there is in Python)
I know the SPI has some overhead, but the device tree file already has the SPI set to 25MHz and the maximum is 50MHz. That should cut the time in half.
I'm trying to figure out how you all intended to use the GPIO mode and what its purpose is for controlling the LO on the ADRV9009 parts. From Travis comment below, it looks like in GPIO mode, an SPI write is still required. Is there something I'm missing here?
Travis said:
In regards to the transceiver itself, you have to follow the steps 1. send SPI write with desired frequency 2. Trigger Move to frequency (GPIO or SPI). Frequency hopping is independent of data that to send or receive.
The UG-1295 says, it takes a minimum of 60us to change the LO frequency depending on the profile settings. Are there any profile settings that can help speed up the change?
I'm trying to get to about 1ms for setting the LO (2ms for both). Is it possible to go this fast in FHM including any SPI communications?
If the SPI communications takes half the time, and the actual trigger and transition takes the other half of the time, i can see how creating a thread to write the next SPI LO frequency and seperate step to trigger the transition could speed things up, but not if the actual transition time is already close to ~60us.
ps How do I reference someone else's comment on this blog? I couldn't find this option.
Please refer to the below and check whether it helps,
https://wiki.analog.com/resources/tools-software/linux-drivers/iio-transceiver/adrv9009#frequency_hopping_mode
I see that the device tree has the GPIO pin set to zero by default (adi,fhm-config-fhm-gpio-pin = <0>).
https://github.com/analogdevicesinc/linux/blob/master/arch/arm64/boot/dts/xilinx/zynqmp-adrv9009-zu11eg-reva.dtsi
It looks like the GPIO referred to in (adi,fhm-cinfig-fhm-gpio-pin) is associated with the 3.3V supply because of this next link. Is this correct?
https://wiki.analog.com/resources/tools-software/linux-drivers/iio-transceiver/adrv9009-customization
From the RFSOM schematic however, there is a little note that says, "AUXDAC_4" on the GPIO_3P3_0_A line. Does the GPIO_3P3_0_A serve as dual purpose in the ADRV9009? I did not see any references in the schematic to FHM GPIO.
How do I write a one or a zero to the GPIO pin, associated with the FHM?
This is what I have tried in Python but it does not cause the LO frequency to trigger and advance after writing the next frequency value via SPI ...
Will be followed here:
https://ez.analog.com/linux-software-drivers/f/q-a/165619/adrv9009-zu11eg-gpio-with-pyadi-iio