Resolution of ADRV9009 ADC on SOM

Hello,

Attached file says that "ADC and DAC Resolution" is "16-bit". (See tabel on top of the 2nd page)

However ADRV9009 datasheet says as below.

AUXILIARY CONVERTERS

- ADC

  - Resolution: 12 Bits

  - Input Voltage

    - Minimum: 0.05 V

    - Maximum: VDDA_ 3P3 - 0.05 V

How should these difference be understood?

I'd like to know these correctly to calculate abusolute received power in dBm from received IQ amplitude.

It means that V/digit is needed for calculation.

Best Regards,

HAL

PDF

Parents Reply Children