ADRV9009 JESD s16p

We are in simulation of JESD204B progress. JESD link is between FPGA (TX) and ADRV9009 (RX). We have all the IBIS-AMI models and package s-parameter files of ADRV9009 and FPGA.

The problem here is the package model of ADRV9009 is s16p and we can not find the document describes these ports are input or output?

Although, we try to setup in 2 cases:

  1. Port 1, 2 are connected to PCB transmission lines and port 3,4 are connected to regenv01_ondie_term.s4pterm.s4p
  2. Port 1, 2 are connected to PCB transmission line and port 9,10 are connected to regenv01_ondie_term.s4pterm.s4p

Based on simulation result, the case 2 seems to be correct setup.

Could you please verify case 2 is correct setup. Or, please let us know what we should do or which document describes about this problem.

Parents
  • +1
    •  Analog Employees 
    on Sep 24, 2019 6:17 AM over 1 year ago

    Talise Design package\IBIS AMI has the "ADRV9009 ADRV9008-1 ADRV9008-2 Serializer IBIS AMI Model Package Description 1.0" document.

    package/AD9379_AD9378-1_AD9378-2_serializer_package_model.s16p

    This touchstone file is used for the package.  It must be placed between the IBIS AMI model instantiation and the channel in the simulation.  The port descriptions are contained in the comments in the beginning of the file.

    Please refer below for port description of ADRV9009_ADRV9008-1_ADRV9008-2_serializer_package_model.s16p,

    ! Created Tue Jul 7 07:54:26 2015
    !
    ! Talise Laminate and Engineering Board : JESD Serializer Path Models.
    ! R0 Production Design.
    !
    ! Upper Metal Layer : Die-UBM.
    ! Lower Metal Layer : Board-M2 (ground).
    ! Includes both "bump" and "ball" models.
    ! Does not include any power distribution models.
    ! Momentum EM Setup:
    ! Sub : Die_UBM_to_B_M2 : Thick Metal.
    ! 3D Modeling, 50 CPW @ 20 Ghz, Edge Mesh, Direct-Dense Solver.
    !
    ! RF Ports:
    ! Port 1 : 3N : Die-UBM.
    ! Port 2 : 3P : Die-UBM.
    ! Port 3 : 1N : Die-UBM.
    ! Port 4 : 1P : Die-UBM.
    ! Port 5 : 2N : Die-UBM.
    ! Port 6 : 2P : Die-UBM.
    ! Port 7 : 0N : Die-UBM.
    ! Port 8 : 0P : Die-UBM.
    ! Port 9 : 3N : Board-M1 Ball Pad.
    ! Port 10 : 3P : Board-M1 Ball Pad.
    ! Port 11 : 2N : Board-M1 Ball Pad.
    ! Port 12 : 2P : Board-M1 Ball Pad.
    ! Port 13 : 1N : Board-M1 Ball Pad.
    ! Port 14 : 1P : Board-M1 Ball Pad.
    ! Port 15 : 0N : Board-M1 Ball Pad.
    ! Port 16 : 0P : Board-M1 Ball Pad.
    !
    ! Frequency Range : 0 Ghz to 32 Ghz.
    ! Frequency Step : 500 Mhz.
    !
    # hz S ma R 50
    ! 16 Port Network Data from data block
    ! freq magS1_1 angS1_1 magS1_2 angS1_2 magS1_3 angS1_3 magS1_4 angS1_4
    ! magS1_5 angS1_5 magS1_6 angS1_6 magS1_7 angS1_7 magS1_8 angS1_8
    ! magS1_9 angS1_9 magS1_10 angS1_10 magS1_11 angS1_11 magS1_12 angS1_12
    ! magS1_13 angS1_13 magS1_14 angS1_14 magS1_15 angS1_15 magS1_16 angS1_16
    ! magS2_1 angS2_1 magS2_2 angS2_2 magS2_3 angS2_3 magS2_4 angS2_4

Reply
  • +1
    •  Analog Employees 
    on Sep 24, 2019 6:17 AM over 1 year ago

    Talise Design package\IBIS AMI has the "ADRV9009 ADRV9008-1 ADRV9008-2 Serializer IBIS AMI Model Package Description 1.0" document.

    package/AD9379_AD9378-1_AD9378-2_serializer_package_model.s16p

    This touchstone file is used for the package.  It must be placed between the IBIS AMI model instantiation and the channel in the simulation.  The port descriptions are contained in the comments in the beginning of the file.

    Please refer below for port description of ADRV9009_ADRV9008-1_ADRV9008-2_serializer_package_model.s16p,

    ! Created Tue Jul 7 07:54:26 2015
    !
    ! Talise Laminate and Engineering Board : JESD Serializer Path Models.
    ! R0 Production Design.
    !
    ! Upper Metal Layer : Die-UBM.
    ! Lower Metal Layer : Board-M2 (ground).
    ! Includes both "bump" and "ball" models.
    ! Does not include any power distribution models.
    ! Momentum EM Setup:
    ! Sub : Die_UBM_to_B_M2 : Thick Metal.
    ! 3D Modeling, 50 CPW @ 20 Ghz, Edge Mesh, Direct-Dense Solver.
    !
    ! RF Ports:
    ! Port 1 : 3N : Die-UBM.
    ! Port 2 : 3P : Die-UBM.
    ! Port 3 : 1N : Die-UBM.
    ! Port 4 : 1P : Die-UBM.
    ! Port 5 : 2N : Die-UBM.
    ! Port 6 : 2P : Die-UBM.
    ! Port 7 : 0N : Die-UBM.
    ! Port 8 : 0P : Die-UBM.
    ! Port 9 : 3N : Board-M1 Ball Pad.
    ! Port 10 : 3P : Board-M1 Ball Pad.
    ! Port 11 : 2N : Board-M1 Ball Pad.
    ! Port 12 : 2P : Board-M1 Ball Pad.
    ! Port 13 : 1N : Board-M1 Ball Pad.
    ! Port 14 : 1P : Board-M1 Ball Pad.
    ! Port 15 : 0N : Board-M1 Ball Pad.
    ! Port 16 : 0P : Board-M1 Ball Pad.
    !
    ! Frequency Range : 0 Ghz to 32 Ghz.
    ! Frequency Step : 500 Mhz.
    !
    # hz S ma R 50
    ! 16 Port Network Data from data block
    ! freq magS1_1 angS1_1 magS1_2 angS1_2 magS1_3 angS1_3 magS1_4 angS1_4
    ! magS1_5 angS1_5 magS1_6 angS1_6 magS1_7 angS1_7 magS1_8 angS1_8
    ! magS1_9 angS1_9 magS1_10 angS1_10 magS1_11 angS1_11 magS1_12 angS1_12
    ! magS1_13 angS1_13 magS1_14 angS1_14 magS1_15 angS1_15 magS1_16 angS1_16
    ! magS2_1 angS2_1 magS2_2 angS2_2 magS2_3 angS2_3 magS2_4 angS2_4

Children