Hello,
I am using the ADRV9009 Evalboard with ZCU102 Board.
I connected the TX and the RX together.
I can receive the sent waveform but the sent RF-pulse does not Start at Time 0.
This is changing from run to run. The reason is, that the TX and the RX are not synchronized.
I want to add a signal to connect the TX to the RX that can be used to synchronize the RX to the TX.
I can think of a trigger signal that sets the receiver memory address to the start-address.
May you please help me find a way to implement this?
Best regards,
Philipp