Two ADRV9009 EVAL Boards on ZCU102

Hi Support,

I want to use two ADRV9009 Eval Boards on ZCU102.

ZCU102 has two FMC(HPC) connectors.

Is it possible to run two ADRV9009 Eval Boards?

Synchronization of  data between two ADRV9009 chips will be OK?

Best Regards.

Tobe 

Parents Reply
  • Hello,

    In my case, the followingis my setup (I am testing it)

    - The second AD9528 doesn't provide REFCLK to FPGA. REFCLK is taken from the first AD9528. But it needs to route from the first board to the second board, then to FPGA through FMC port (to provide REF for GT Transceiver)

    - SYSREF for AD9009 on the second board, on the other hand, is still provided by the second AD9528 (in bypass mode - source is from 1st AD9528), then I can adjust its delay.

    - SYSREF for FPGA side just need to be taken from 1st AD9528.

    P/S: I think you should start another thread, so we can discuss further and get more support from ADI.

    Regards,

    Trung Nguyen

Children