We have a customer looking to add JTAG boundary scan on a dual ADRV9004 design.
ADRV9004 RevA datasheet pg. 95 and Table 19 (pg. 96) seems to be the only info about JTAG - nothing in the UG, rev PrC. It shows that pins DGPIO_3-11 are used, along with the MODE pin, and these DGPIOs are already deployed in their design.
So they ask:
1) Can these DGPIOs simply be branched to the JTAG connector without termination concerns, or is there a preferred way to maintain signal integrity?
2) What's the best way to connect two devices to the JTAG bus? - e.g. TDI's and TDO's each paralleled or daisy-chained with a TDI--TDO loop, with a TDO--TDI connection between devices? (These would be the only two devices on the JTAG bus with the connector.)
3) How do you recommend separating the DGPIOs of each device [for conventional/independent GPIO use] when not in JTAG mode? Tri-state buffers or switches or ??