Post Go back to editing

Question of ADRV9002 Tx power detector and sampling rate

Category: Software
Product Number: adrv9002

I have 3 questions about ADRV9002 as below.
I know that RSSI can be measured in the Rx path.

1) Is it possible to measure Tx power in Tx signal path? Also, which API function should I use?

2) Is there an API function that can check the status of DPD execution?

3) I have a table like below in the datasheet.

When selecting the interface mode of LSSI in 2-lane data, can I change the sampling rate for I and Q data to 86MHz?

Please help us with the above three questions.

thank you.

Parents Reply Children