Hi,
I would like to monitor ADRV9002 power consumption from on board ADM1293. TES power monitor function is not enough time scale and resolution. So, I would like to try to read it by C code implementation.(Use C code generation function and TES SD card)
ADRV900x C code library has ADM1293 read function. I think TES used this code.
Can I have any sample code or reference design about power monitoring function for implementing my C code?
And also, if possible, I would like to read the power value as fast as possible. In the datasheet, ADM1293 has conversion speed that is around 100us. So, I think it will be several ksps max.
If you have any limitation about read cycle the power from ADM1293, I would like to have the spec about Evaluation board.
I'm not sure the read cycle of TES power monitor function. If ADM1293 read cycle limitation is similar with TES spec, I can understand the limitation.
Best regards,
Jun