Issue with AD9371 uboot and kernel image load

If you are facing errors while booting the Linux kernel shipped along with SD card, follow these steps to correctly set uboot.

  • Connect a USB mini cable between your computer and the ZC706 board UART port
  • Open a Tera Term window (or equivalent tool) and connect to the proper UART port
  • Turn on the ZC706 board and stop the autoboot when prompted
  • Enter the following command:  env default –a
  • Enter the following command: saveenv
  • Enter the following command: reset

 

This process should ensure the ZC706 has the proper uboot loaded into the flash memory on the board.