Post Go back to editing

AD9371 ORx Gain Table changing Index does not change gain

Good day!

I am using the AD9371 transceiver API for No-OS from the ADI GIT master branch

github.com/.../ad9371

Where the provided ORx Gain Table is written into the transceiver.


I am having an issue with MYKONOS_setObsRxManualGain() where it does not work as expected that despite using different indices within the ORx Gain Table range,
there were no observed changes in the operation of the AD9373 transceiver.

Is there a requirement, a function that needs to enabled or disabled before executing the function?

also, I noticed from mykonos_user.h, ln43:

#define MIN_ORX_GAIN_TABLE_INDEX (MAX_GAIN_TABLE_INDEX - START_ORX_GAIN_INDEX) /* 255 - 47 = 208

if calculated, MIN_ORX_GAIN_TABLE_INDEX gives out a min index of 208 yet ORxGainTable[19][4] is captioned to have a min index of 237.
is there a reason for START_ORX_GAIN_INDEX = 47?

Thank you.

Parents Reply Children