Hi,
I am trying to modify the Transmit and Receive LTE MIMO code given in the below link.
https://www.mathworks.com/help/supportpkg/xilinxzynqbasedradio/examples/transmit-and-receive-lte-mimo-using-a-single-analog-devices-ad9361-ad9364.html
This code runs perfectly on AD RF SOM.
Now, I am trying the same example to run on ADRV9371.
ad9361_LTE() ( The code that's in the Legacy folder under LTE_MATLAB) uses IIO hence, I modified this code to 9371 and it works for the dummy data which is used in trData. (I was able to see LTE spectrum on the Spectrum Analyzer). Please note that I upsampled the enodeBOutput by 8 (to match 122.88Mhz) for Transnmission.
But, when I modify it to the above image and try to Transmit, MATLAB crashes. After a bit debugging, I understood that the buffer size that I have pre-allocated,is too large and that could be the reason for my Crash. (Not sure though)
Next, I changed the IIO objects to Adi Objects and used adi.AD9371.Tx and could similarly transmit the dummy Data but, when tried to Transmit the full grid, I get an error.
This error is related to SamplesPerFrame. The Final enodeBOutput is much larger than 2^20, Hence,I always get an error.
How, do I transmit this whole grid either using IIO objects or ADI objects?
Please suggest any work around.
Regards
sravan
Error
Error using adi.AD9371.Base/set.SamplesPerFrame (line 65)Expected SamplesPerFrame to be a scalar with value <= 1.04858e+06.
Error in adi.AD9371.Tx/setupImpl (line 71) obj.SamplesPerFrame = size(data,1);
Error in ad9371_LTE_adi_Tx_3 (line 216)tx(eNodeBOutput);
There is a maximum bound on the samples you can transmit without modify HDL and the linux kernel. The bound we pre-set in the system object is conservative (2^20). You can try increasing this changing the value on this line: https://github.com/analogdevicesinc/MathWorks_tools/blob/master/%2Badi/%2BAD9371/Base.m#L66
It may be possible to extend this to 2^23.
-Travis
Hi Travis, also another question.
How can I modify the HDL and linux kernel? Can you please point me to some documentation?
Are you handling the default rate differences between RX and TX?
Hi Travis,
I am using the filter profile given in GitHub. When I loaded the profile into TES, it says the Tx rate and Rx rate are same ie; 122.88Mhz.
Aren't they same?
Even if they were not same I tried capturing twice the samples as TX but still I don't see an change.
By default, TX is 2x RX, but if you are using a profile where they are the same, that should be fine.
Have you visually inspected the signal in both time and frequency to get what you expect?
Are you using cyclic buffers on the TX?
I tried to save the final output into a text file and load in TES. but I guess there is a limit on file size so it always pops an error message file not found.(the file size is around 63 MB).
I truncated the output to one frame ie:153600*8 since my upsampling factor is 8.
I see a frame on the receive data as expected, in frequency domain.
Yes, I am enabling the cyclic buffers.
And, in the receiver side, I flush the buffers as it was did in example codes.
Can you provide your MATLAB script?
%% Transmitter %% ad971_LTE_adi_Tx_singlecarrier close all; clc; clear; %% %ip = '192.168.3.2'; LTEmode = 'LTE10'; %load eNBupsampfilter.mat; %% % Setup handle for image plot if ~exist('imFig', 'var') || ~ishandle(imFig) imFig = figure; imFig.NumberTitle = 'off'; imFig.Name = 'Image Plot'; imFig.Visible = 'off'; else clf(imFig); % Clear figure imFig.Visible = 'off'; end % Setup handle for channel estimate plots if ~exist('hhest', 'var') || ~ishandle(hhest) hhest = figure('Visible','Off'); hhest.NumberTitle = 'off'; hhest.Name = 'Channel Estimate'; else clf(hhest); % Clear figure hhest.Visible = 'off'; end % Setup Spectrum viewer spectrumScope = dsp.SpectrumAnalyzer( ... 'SpectrumType', 'Power density', ... 'SpectralAverages', 10, ... 'YLimits', [-135 -45], ... 'Title', 'Received Baseband LTE Signal Spectrum', ... 'YLabel', 'Power spectral density'); % Setup the constellation diagram viewer for equalized PDSCH symbols constellation = comm.ConstellationDiagram('Title','Equalized PDSCH Symbols',... 'ShowReferenceConstellation',false); %% Pick up LTE parameters according to LTE Mode if strcmp(LTEmode,'LTE1.4') == 1 configuration = 'R.4'; samplingrate = 1.92e6; bandwidth = 1.08e6; fir_data_file = 'LTE1p4_MHz.ftr'; elseif strcmp(LTEmode,'LTE3') == 1 configuration = 'R.5'; samplingrate = 3.84e6; bandwidth = 2.7e6; fir_data_file = 'LTE3_MHz.ftr'; elseif strcmp(LTEmode,'LTE5') == 1 configuration = 'R.6'; samplingrate = 7.68e6; bandwidth = 4.5e6; fir_data_file = 'LTE5_MHz.ftr'; elseif strcmp(LTEmode,'LTE10') == 1 configuration = 'R.7'; samplingrate = 15.36e6; bandwidth = 9e6; fir_data_file = 'LTE10_MHz.ftr'; else error('Please input LTE1.4, LTE3, LTE5 or LTE10.'); end uri = 'ip:192.168.3.2'; %fc = 0.7e9; %% Generate LTE Signal using LTE System Toolbox % Check for LST presence if isempty(ver('lte')) error('ad9361_LTE:NoLST','Please install LTE System Toolbox to run this example.'); end % Generate the LTE signal txsim.RC = configuration; % Base RMC configuration txsim.NCellID = 143; % Cell identity txsim.NFrame = 700; % Initial frame number txsim.TotFrames = 1; % Number of frames to generate txsim.RunTime = 200; % Time period to loop waveform in seconds %%% Changing this RunTime to 2000 did'nt have any effect, Initially it was 20 txsim.DesiredCenterFrequency = 2.45e9; % Center frequency in Hz txsim.NTxAnts = 1; %% Prepare Tx Image % Input an image file and convert to binary stream fileTx = 'peppers.png'; % Image file name fData = imread(fileTx); % Read image data from file scale = 0.5; % Image scaling factor origSize = size(fData); % Original input image size scaledSize = max(floor(scale.*origSize(1:2)),1); % Calculate new image size heightIx = min(round(((1:scaledSize(1))-0.5)./scale+0.5),origSize(1)); widthIx = min(round(((1:scaledSize(2))-0.5)./scale+0.5),origSize(2)); fData = fData(heightIx,widthIx,:); % Resize image imsize = size(fData); % Store new image size binData = dec2bin(fData(:),8); % Convert to 8 bit unsigned binary trData = reshape((binData-'0').',1,[]).'; % Create binary stream %% Display Tx Image % Plot transmit image figure(imFig); imFig.Visible = 'on'; subplot(211); imshow(fData); title('Transmitted Image'); subplot(212); title('Received image will appear here...'); set(gca,'Visible','off'); % Hide axes set(findall(gca, 'type', 'text'), 'visible', 'on'); % Unhide title pause(1); % Pause to plot Tx image %% Create RMC % Generate RMC configuration and customize parameters rmc = lteRMCDL(txsim.RC); %% % Calculate the required number of LTE frames based on the size of the % image data trBlkSize = rmc.PDSCH.TrBlkSizes; txsim.TotFrames = ceil(numel(trData)/sum(trBlkSize(:))); rmc.NCellID = txsim.NCellID; rmc.NFrame = txsim.NFrame; rmc.TotSubframes = txsim.TotFrames*10; % 10 subframes per frame rmc.CellRefP = txsim.NTxAnts; % Configure number of cell reference ports rmc.PDSCH.RVSeq = 0; % Add noise to unallocated PDSCH resource elements if verLessThan('matlab','9.2') rmc.OCNG = 'On'; else rmc.OCNGPDSCHEnable = 'On'; rmc.OCNGPDCCHEnable = 'On'; end fprintf('\nGenerating LTE transmit waveform:\n') fprintf(' Packing image data into %d frame(s).\n\n', txsim.TotFrames); % Pack the image data into a single LTE frame [eNodeBOutput,txGrid,rmc] = lteRMCDLTool(rmc,trData); %txsim.SamplingRate = rmc.SamplingRate; % Scale the signal for better power output and cast to int16. This is the % native format for the SDR hardware. Since we are transmitting the same % signal in a loop, we can do the cast once to save processing time. powerScaleFactor = 0.7; eNodeBOutput = eNodeBOutput.*(1/max(abs(eNodeBOutput))*powerScaleFactor); eNodeBOutput = resample(eNodeBOutput,8,1); %eNodeBOutput1 = filter(eNBupsampfilter,1,eNodeBOutput); figure(); pwelch(eNodeBOutput,[],[],[],15.36e6*8,'centered'); title('Spectrum of Upsampled eNodeBOutput') % figure(); % pwelch(eNodeBOutput1,[],[],[],15.36e6*8,'centered'); % title('Spectrum of Upsampled and filtered eNodeBOutput1') % Cast the transmit signal to int16 --- % this is the native format for the SDR hardware. %%%%%%%%%%%%%%%%%%%%%% eNodeBOutput = int16(eNodeBOutput*2^15); %% Tx set up tx = adi.AD9371.Tx('uri',uri); tx.CenterFrequency = txsim.DesiredCenterFrequency; tx.EnableCustomProfile = true; tx.CustomProfileFileName = 'profile_TxBW100_ORxBW100_RxBW100.txt'; tx.DataSource = 'DMA'; tx.EnableCyclicBuffers = true; tx.AttenuationChannel0 = 0; %save ('allvbles.mat'); %pause(2); tx(eNodeBOutput);
%% Receiver %% ad971_LTE_adi_Rx_singlecarrier %% User defined parameters --- configure the same as transmitter %% %load allvbles.mat %load rxfilter_30pi72M.mat %load rxfilter_15pi36M.mat osf=8; rxsim = struct; rxsim.RadioFrontEndSampleRate = samplingrate*osf;%tx.BasebandSampleRate; % Configure for same sample rate % as transmitter rxsim.RadioCenterFrequency = txsim.DesiredCenterFrequency; rxsim.NRxAnts = txsim.NTxAnts; rxsim.FramesPerBurst = txsim.TotFrames+1; % Number of LTE frames to capture in each burst. % Capture 1 more LTE frame than % transmitted to allow for timing % offset wraparound... rxsim.numBurstCaptures = 1; % Number of bursts to capture % Derived parameters samplesPerFrame = 10e-3*rxsim.RadioFrontEndSampleRate/osf; % LTE frames period is 10 ms %An SDR Receiver system object is used with the named radio 'AD936x' to %receive baseband data from the SDR hardware. sdrReceiver = adi.AD9371.Rx('uri',uri); sdrReceiver.CenterFrequency = rxsim.RadioCenterFrequency; sdrReceiver.SamplesPerFrame = samplesPerFrame*osf; %% Capture 6 frames of this length to decode sdrReceiver.GainControlMode = 'automatic'; %% burstCaptures holds sdrReceiver.FramesPerBurst number of consecutive frames worth % of baseband LTE samples. Each column holds one LTE frame worth of data. burstCaptures = zeros(samplesPerFrame*osf,rxsim.NRxAnts,rxsim.FramesPerBurst); enb.PDSCH = rmc.PDSCH; enb.DuplexMode = 'FDD'; enb.CyclicPrefix = 'Normal'; enb.CellRefP = 4; % Bandwidth: {1.4 MHz, 3 MHz, 5 MHz, 10 MHz, 20 MHz} SampleRateLUT = [1.92 3.84 7.68 15.36 30.72]*1e6; NDLRBLUT = [6 15 25 50 100]; enb.NDLRB = NDLRBLUT(SampleRateLUT==rxsim.RadioFrontEndSampleRate/osf); if isempty(enb.NDLRB) error('Sampling rate not supported. Supported rates are %s.',... '1.92 MHz, 3.84 MHz, 7.68 MHz, 15.36 MHz, 30.72 MHz'); end fprintf('\nSDR hardware sampling rate configured to capture %d LTE RBs.\n',enb.NDLRB); %% Channel estimation configuration structure cec.PilotAverage = 'UserDefined'; % Type of pilot symbol averaging cec.FreqWindow = 9; % Frequency window size in REs cec.TimeWindow = 9; % Time window size in REs cec.InterpType = 'Cubic'; % 2D interpolation type cec.InterpWindow = 'Centered'; % Interpolation window type cec.InterpWinSize = 3; % Interpolation window size enbDefault = enb; %% % Setup Spectrum viewer spectrumScope = dsp.SpectrumAnalyzer( ... 'SpectrumType', 'Power density', ... 'SpectralAverages', 10, ... 'YLimits', [-60 80], ... 'Title', 'Received Baseband LTE Signal Spectrum', ... 'YLabel', 'Power spectral density'); %% for i=1:20 sdrReceiver(); end %% Receive, detect and decode packet while rxsim.numBurstCaptures % Set default LTE parameters enb = enbDefault; % SDR Capture fprintf('\nStarting a new RF capture.\n\n') len=0; for frame = 1:rxsim.FramesPerBurst while len == 0 % Store one LTE frame worth of samples [data,len] = sdrReceiver(); end burstCaptures(:,:,frame) = data;%((frame-1)*frameLen+1:frameLen*frame); end %burstCapturesadi = burstCaptures; % only for debugging if rxsim.NRxAnts == 2 rxWaveform = reshape(permute(burstCaptures,[1 3 2]), ... rxsim.FramesPerBurst*samplesPerFrame,rxsim.NRxAnts); spectrumScope.ShowLegend = true; % Turn on legend for spectrum analyzer spectrumScope.ChannelNames = {'SDR Channel 1','SDR Channel 2'}; else % Downsample the received signal rxWaveform = resample(burstCaptures(:),1,osf); %rxWaveform = filter(rxfilter_15pi36M,1,rxWaveform); %rxWaveform = filter(rxfilter_30pi72M,1,rxWaveform); % figure(); % pwelch(rxWaveform,[],[],[],15.36e6,'centered'); % title(' Spectrum After DownSampling') end %%%%%%%%%% After resampling shouldn't we use LowPass filetring%%%% % Show power spectral density of captured burst spectrumScope.SampleRate = rxsim.RadioFrontEndSampleRate/(osf); spectrumScope(rxWaveform); % Perform frequency offset correction for known cell ID frequencyOffset = lteFrequencyOffset(enb,rxWaveform); rxWaveform = lteFrequencyCorrect(enb,rxWaveform,frequencyOffset); fprintf('\nCorrected a frequency offset of %i Hz.\n',frequencyOffset) % Perform the blind cell search to obtain cell identity and timing offset % Use 'PostFFT' SSS detection method to improve speed cellSearch.SSSDetection = 'PostFFT'; cellSearch.MaxCellCount = 1; [NCellID,frameOffset] = lteCellSearch(enb,rxWaveform,cellSearch); fprintf('Detected a cell identity of %i.\n', NCellID); enb.NCellID = NCellID; % From lteCellSearch % Sync the captured samples to the start of an LTE frame, and trim off % any samples that are part of an incomplete frame. rxWaveform = rxWaveform(frameOffset+1:end,:); tailSamples = mod(length(rxWaveform),samplesPerFrame); rxWaveform = rxWaveform(1:end-tailSamples,:); enb.NSubframe = 0; fprintf('Corrected a timing offset of %i samples.\n',frameOffset) % OFDM demodulation rxGrid = lteOFDMDemodulate(enb,rxWaveform); % Perform channel estimation for 4 CellRefP as currently we do not % know the CellRefP for the eNodeB. [hest,nest] = lteDLChannelEstimate(enb,cec,rxGrid); sfDims = lteResourceGridSize(enb); Lsf = sfDims(2); % OFDM symbols per subframe LFrame = 10*Lsf; % OFDM symbols per frame numFullFrames = length(rxWaveform)/samplesPerFrame; rxDataFrame = zeros(sum(enb.PDSCH.TrBlkSizes(:)),numFullFrames); recFrames = zeros(numFullFrames,1); rxSymbols = []; txSymbols = []; % For each frame decode the MIB, PDSCH and DL-SCH for frame = 0:(numFullFrames-1) fprintf('\nPerforming DL-SCH Decode for frame %i of %i in burst:\n', ... frame+1,numFullFrames) % Extract subframe #0 from each frame of the received resource grid % and channel estimate. enb.NSubframe = 0; rxsf = rxGrid(:,frame*LFrame+(1:Lsf),:); hestsf = hest(:,frame*LFrame+(1:Lsf),:,:); % PBCH demodulation. Extract resource elements (REs) % corresponding to the PBCH from the received grid and channel % estimate grid for demodulation. enb.CellRefP = 4; pbchIndices = ltePBCHIndices(enb); [pbchRx,pbchHest] = lteExtractResources(pbchIndices,rxsf,hestsf); [~,~,nfmod4,mib,CellRefP] = ltePBCHDecode(enb,pbchRx,pbchHest,nest); % If PBCH decoding successful CellRefP~=0 then update info if ~CellRefP fprintf(' No PBCH detected for frame.\n'); continue; end enb.CellRefP = CellRefP; % From ltePBCHDecode % Decode the MIB to get current frame number enb = lteMIB(mib,enb); % Incorporate the nfmod4 value output from the function % ltePBCHDecode, as the NFrame value established from the MIB % is the system frame number modulo 4. enb.NFrame = enb.NFrame+nfmod4; fprintf(' Successful MIB Decode.\n') fprintf(' Frame number: %d.\n',enb.NFrame); % The eNodeB transmission bandwidth may be greater than the % captured bandwidth, so limit the bandwidth for processing enb.NDLRB = min(enbDefault.NDLRB,enb.NDLRB); % Store received frame number recFrames(frame+1) = enb.NFrame; % Process subframes within frame (ignoring subframe 5) for sf = 0:9 if sf~=5 % Ignore subframe 5 % Extract subframe enb.NSubframe = sf; rxsf = rxGrid(:,frame*LFrame+sf*Lsf+(1:Lsf),:); % Perform channel estimation with the correct number of CellRefP [hestsf,nestsf] = lteDLChannelEstimate(enb,cec,rxsf); % PCFICH demodulation. Extract REs corresponding to the PCFICH % from the received grid and channel estimate for demodulation. pcfichIndices = ltePCFICHIndices(enb); [pcfichRx,pcfichHest] = lteExtractResources(pcfichIndices,rxsf,hestsf); [cfiBits,recsym] = ltePCFICHDecode(enb,pcfichRx,pcfichHest,nestsf); % CFI decoding enb.CFI = lteCFIDecode(cfiBits); % Get PDSCH indices [pdschIndices,pdschIndicesInfo] = ltePDSCHIndices(enb, enb.PDSCH, enb.PDSCH.PRBSet); [pdschRx, pdschHest] = lteExtractResources(pdschIndices, rxsf, hestsf); % Perform deprecoding, layer demapping, demodulation and % descrambling on the received data using the estimate of % the channel [rxEncodedBits, rxEncodedSymb] = ltePDSCHDecode(enb,enb.PDSCH,pdschRx,... pdschHest,nestsf); % Append decoded symbol to stream rxSymbols = [rxSymbols; rxEncodedSymb{:}]; %#ok<AGROW> % Transport block sizes outLen = enb.PDSCH.TrBlkSizes(enb.NSubframe+1); % Decode DownLink Shared Channel (DL-SCH) [decbits{sf+1}, blkcrc(sf+1)] = lteDLSCHDecode(enb,enb.PDSCH,... outLen, rxEncodedBits); %#ok<SAGROW> % Recode transmitted PDSCH symbols for EVM calculation % Encode transmitted DLSCH txRecode = lteDLSCH(enb,enb.PDSCH,pdschIndicesInfo.G,decbits{sf+1}); % Modulate transmitted PDSCH txRemod = ltePDSCH(enb, enb.PDSCH, txRecode); % Decode transmitted PDSCH [~,refSymbols] = ltePDSCHDecode(enb, enb.PDSCH, txRemod); % Add encoded symbol to stream txSymbols = [txSymbols; refSymbols{:}]; %#ok<AGROW> release(constellation); % Release previous constellation plot constellation(rxEncodedSymb{:}); % Plot current constellation pause(0); % Allow constellation to repaint end end % Reassemble decoded bits fprintf(' Retrieving decoded transport block data.\n'); rxdata = []; for i = 1:length(decbits) if i~=6 % Ignore subframe 5 rxdata = [rxdata; decbits{i}{:}]; %#ok<AGROW> end end % Store data from receive frame rxDataFrame(:,frame+1) = rxdata; % Plot channel estimate between CellRefP 0 and the receive antennae focalFrameIdx = frame*LFrame+(1:LFrame); figure(hhest); hhest.Visible = 'On'; surf(abs(hest(:,focalFrameIdx,1,1))); shading flat; xlabel('OFDM symbol index'); ylabel('Subcarrier index'); zlabel('Magnitude'); title('Estimate of Channel Magnitude Frequency Repsonse'); end rxsim.numBurstCaptures = rxsim.numBurstCaptures-1; % release(spectrumScope); % % Setup Spectrum viewer % spectrumScope = dsp.SpectrumAnalyzer( ... % 'SpectrumType', 'Power density', ... % 'SpectralAverages', 10, ... % 'YLimits', [-135 -45], ... % 'Title', 'Received Baseband LTE Signal Spectrum', ... % 'YLabel', 'Power spectral density'); end % Release both the transmitter and receiver objects once reception is complete %release(sdrTransmitter); release(tx); release(sdrReceiver); %% Determine index of first transmitted frame (lowest received frame number) [~,frameIdx] = min(recFrames); fprintf('\nRecombining received data blocks:\n'); decodedRxDataStream = zeros(length(rxDataFrame(:)),1); frameLen = size(rxDataFrame,1); % Recombine received data blocks (in correct order) into continuous stream for n=1:numFullFrames currFrame = mod(frameIdx-1,numFullFrames)+1; % Get current frame index decodedRxDataStream((n-1)*frameLen+1:n*frameLen) = rxDataFrame(:,currFrame); frameIdx = frameIdx+1; % Increment frame index end % Perform EVM calculation if ~isempty(rxSymbols) evmCalculator = comm.EVM(); evmCalculator.MaximumEVMOutputPort = true; [evm.RMS,evm.Peak] = evmCalculator(txSymbols, rxSymbols); fprintf(' EVM peak = %0.3f%%\n',evm.Peak); fprintf(' EVM RMS = %0.3f%%\n',evm.RMS); else fprintf(' No transport blocks decoded.\n'); end % Perform bit error rate (BER) calculation bitErrorRate = comm.ErrorRate; err = bitErrorRate(decodedRxDataStream(1:length(trData)), trData); fprintf(' Bit Error Rate (BER) = %0.5f.\n', err(1)); fprintf(' Number of bit errors = %d.\n', err(2)); fprintf(' Number of transmitted bits = %d.\n',length(trData)); % Recreate image from received data fprintf('\nConstructing image from received data.\n'); str = reshape(sprintf('%d',decodedRxDataStream(1:length(trData))), 8, []).'; decdata = uint8(bin2dec(str)); receivedImage = reshape(decdata,imsize); % Plot receive image if exist('imFig', 'var') && ishandle(imFig) % If TX figure is open figure(imFig); subplot(212); else figure; subplot(212); end imshow(receivedImage); title(sprintf('Received Image: %dx%d Antenna Configuration',txsim.NTxAnts, rxsim.NRxAnts));
Please find the attached code. I couldn't attach a zip file or .m file.
In the transmitter please use the profile 'profile_TxBW100_ORxBW100_RxBW100.txt';
please let me know if you need any files while running
Have you got an opportunity to go through the codes?
please let me know if there are any problems in the codes?
Thanks in advance
I don't have a board on me right now, but looking at the code RX data is 1/5 the size of a TX frame. "burstCaptures" should be 2*length(eNodeBOutput).
Make sure you set a profile on the RX side too.
Now, I set the RX profile as well.
Now, I get cellID correctly.
But, I am only able to decode either one or two frames. and each time I run, the frame number that are decoded correctly changes. like 700&704 or 701&702 like wise or only 703 will be decoded.
I'm Attaching the Command Prompt results at the end.
Note:
The length(eNodeBoutput) in Tx is 153600*5*8 ie; 6144000
burstcaptures in receiver is 153600*8*6. I receive one frame more than Tx . Its not 1/5 of Tx.
Also,As per suggestion, I tried to receive twice the length(eNodeBoutPut) in receiver but even then, only one/two frames are decode properly as said above.
Run1 :
Run 2:
Hi travis,
I fixed the issue. The problem was, as soon as I call the receiver the transmitter is being released even though I had enabled the cyclic buffers.
In the receiver code above, the loop for this is
for frame = 1:rxsim.FramesPerBurst while len == 0 % Store one LTE frame worth of samples [data,len] = sdrReceiver(); end burstCaptures(:,:,frame) = data; %((frame-1)*frameLen+1:frameLen*frame);
I connected a splitter and connected one of the output to spectrum analyzer and the other for tx and rx loop back..
I set a breakpoint at the receiver call ( data,len] = sdrReceiver();), and as soon as i step forward i don't see any spectrum. and rest all calls its only taking some junk.
I captured the entire burst sizes that I need for decoding instead of looping for six times and it worked.
But, it was strange,why the receiver call is releasing the transmitter?
please let me know if this is the way it is programmed.
thanks for the advices.