I want to generate LTE signal with sampling rate of 122.88MSPS for testing using AD9371 Evalution board using ZC706 zynq board & IIO Scope.
First I generated LTE test signal using LTE Downlink Generator App in matlab & then upsampled to get 122.88MHz. After uploading that file in DAC Buffer in IIO scope, i was getting little different waveform than ideal.
I have written matlab code for upsampling as
sig_out = resample(x, 4, 1);
>> db_backoff = 3;
>> QAM64_20MHz = tmwaveform * (10^(-db_backoff/20))/max([max(real(tmwaveform)) abs(min(real(tmwaveform))) max(imag(tmwaveform)) abs(min(imag(tmwaveform)))]);
Pls suggest
Pls suggest what to do toget ideal waveform.
Please refer to the below link:
https://ez.analog.com/wide-band-rf-transceivers/design-support-ad9371/f/q-a/108332/create-waveform-for-ad9371-in-matlab/334881#334881