With a CW Rx Input at the AD9371 Maximum Recommended Input Power of -14 dBm and no internal Rx attenuation (Gain Table Index = 255) what is the expected digital signal power in dBFS?
Are these calculations correct?
-14 dBm : External CW Input
0 dB : AD9371 Rx Adjustable Attenuation
+18 dB : AD9371 Rx Fixed Internal Gain
-7 dB : ADC dBm to dBFS (Full scale ADC input is +7 dBm)
-------------
-3 dBFS : expected digital signal power
Also, what is the expected Tx Output power of a 0 dBFS CW tone with no internal Tx attenuation?
thanks.