ARM Command Error in MYKONOS_setRfPllFrequency() when building the no-os project with ad937

Hello,

I am following the guide in https://wiki.analog.com/resources/eval/user-guides/mykonos/no-os-setup with my zc706 and ad9371. However I come across this error ARM Command Error in MYKONOS_setRfPllFrequency(), the message is shown in the picture below. The code I use is in the .rar below. I follow the guide to generate all of the codes, and simply modified it according to https://ez.analog.com/wide-band-rf-transceivers/tes-gui-and-api-software-ad9371-ad9375/f/q-a/102045/ad9528_initialize-issues-possible-cause-ref_clk-not-connected so it is really hard for me to solve this error. Hoping someone could help me with this problem.

 zc706_4.rar