ADC synchronization between AD9375s

Hello,

We want to use four AD9375s to achieve 8 * 8 MIMO and we need the ADC synchronization between two AD9375s.

Can it achieve synchronous sampling between the ADCs in two chips?

Thank you 

  • Baseband synchronization can be achieved through multichip synchronization (MCS) features. Note that MCS function does not include RF synchronization. The ability to synchronize RF local oscillators (LOs) is not available in the device. The only alignment among multiple chips that is possible using this feature is digital timing alignment.  Consult the user guide for more information on MCS (UG-992).

    -Travis