Post Go back to editing

Ad9371 Frequency change and Noise Floor

hi,

i am totally new in this field and new some help.
i have 3 question about the ad9371 transceiver ic.
i. How to change the central Frequency in run time and how much time it will take to shift?
ii. what is the noise floor value at RX end at -80 dB, as this ic has sensitivity of -80dB.
iii. How can i reduce the bandwidth (RX side only) without slow down the IQ data rate. (in form at analog.com i found that it may be not possible) kindly explain.
i am new to this domain and still learning we are working with a AD9371 no-OS application currently.
thanks in advance

regards
Asad Asif

Top Replies

  • i. How to change the central Frequency in run time and how much time it will take to shift?

    The VCO calibration plus lock time will take approximately 260µs worst case.

    ii. what…
Parents Reply
  • So, you need to hop the LO frequency to 2.4GHz+/-8MHz?  Fast frequency hoping is not supported by AD9371. You can use AD9361 for that. In fast lock mode, the LO hop time is reduced to 20usec. Refer to the fast lock section in AD9361 UG for details on doing that.

Children