Ad9371 Frequency change and Noise Floor

hi,

i am totally new in this field and new some help.
i have 3 question about the ad9371 transceiver ic.
i. How to change the central Frequency in run time and how much time it will take to shift?
ii. what is the noise floor value at RX end at -80 dB, as this ic has sensitivity of -80dB.
iii. How can i reduce the bandwidth (RX side only) without slow down the IQ data rate. (in form at analog.com i found that it may be not possible) kindly explain.
i am new to this domain and still learning we are working with a AD9371 no-OS application currently.
thanks in advance

regards
Asad Asif

Parents Reply
  • Good day sir,

    sir i wanna to know if it is possible with AD9371 putting TX LO at fix frequency and then hop to a near by frequency within the TX bandwidth (TX has 100 MHz bandwidth) without changing the central frequency of Tx.

    regards

    Asad Asif

Children