For the AD9371 ... can i use the RX and oRX input simulation at 100MHz (Rx) and 250MHz (oRx) with different LO-frequencies?
AD9371
Recommended for New Designs
The AD9371 is a highly integrated, wideband RF transceiver
offering dual channel transmitters and receivers, integrated synthesizers, and digital signal...
Datasheet
AD9371 on Analog.com
For the AD9371 ... can i use the RX and oRX input simulation at 100MHz (Rx) and 250MHz (oRx) with different LO-frequencies?
On behalf of Wyatt Taylor: Yes, that is a valid mode for the AD9371.
On behalf of Wyatt Taylor: Yes, that is a valid mode for the AD9371.