Post Go back to editing

06-15-17 What is the definition difference between BW and Synthesis BW on the slide for AD9375?

What is the definition difference between BW and Synthesis BW on the slide for AD9375?

Parents
  • On behalf of Peadar Forbes:

    "Bandwidth” is the signal bandwidth that is supported, e.g. 20MHz LTE or 2x20MHz LTE. That is limited to 40MHZ with this DPD solution. The synthesis bandwidth is the bandwidth over which predistortion energy is output to correct PA non-linearities. That can be as high as 250MHz with the AD9375.

Reply
  • On behalf of Peadar Forbes:

    "Bandwidth” is the signal bandwidth that is supported, e.g. 20MHz LTE or 2x20MHz LTE. That is limited to 40MHZ with this DPD solution. The synthesis bandwidth is the bandwidth over which predistortion energy is output to correct PA non-linearities. That can be as high as 250MHz with the AD9375.

Children
No Data