What solder-ability risks are there from uncontrolled storage and only baking before use, particularly in a high humidity environment?
KCC's Quizzes AQQ305 about a mutual exponentiation equation
1. Quote of the month: "A train station is where a train stops. A bus station is where a bus stops. I have a work station on my desk, so..." - unknown
2. Quiz AQQ305 about finding a mutual exponential equation
Good luck, and try to be among the
View All
September Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Quiz: How Well Do You Know Adaptive Power Switching?
Is your I/O module overheating? The AD74416H's Adaptive Power Switching (APS) can cut heat dissipation by up to 40% — but how well do you really understand how it works?
Read the blog first: Cooling
View All
What solder-ability risks are there from uncontrolled storage and only baking before use, particularly in a high humidity environment?
If products are stored outside dry-packs in a high humidity environment, they can absorb moisture between the leads and the package. If the devices are not completely baked out according to industry standards, that moisture can boil during solder re-flow and pop the package open. Also, if the packages are left exposed for an extended period, the leads on the package may oxidize, which will result in unreliable solder joints in assembly. Lead oxidation will not be reversed by bake-out. Lead oxidization can be removed with flux, but this is a tedious procedure not suitable for volume assembly.