Say, if the specs are at 5 V and 25 °C and I have to use the part at 7.5 V and 50 °C and I have two separate curves for voltage and temperature, how can I combine them?
KCC's Quizzes AQQ304 - A pure logic
1. Quote of the month: "I am not lazy, I'm just in energy-saving mode" - unknown
2. Quiz AQQ304 about finding a pure logic puzzle
Mike is looking at Anne, but Anne is looking at Paul.
Mike is married, but Paul is not.
Question:
Is a married
View All
August Monthly Blog Quiz! Read the blog, take the quiz, and you could win a gift card
Important: Read the blog first . The quiz questions are all based on the content of the blog:
Stay in the loop and win! Read the blog Current Output Driving Industrial Loops , then take our quick five-question quiz for a chance to win a gift card
View All
Say, if the specs are at 5 V and 25 °C and I have to use the part at 7.5 V and 50 °C and I have two separate curves for voltage and temperature, how can I combine them?
Every product is different -- so there isn't an answer that will fit every case. You can call our tech support operation or send an email through the contacts on the web site about the product you are interested in.
Every product is different -- so there isn't an answer that will fit every case. You can call our tech support operation or send an email through the contacts on the web site about the product you are interested in.